Tool/software:
We understood that with Qg and Tsw we could estimate the Igate, that would be the discharge current of bootstrap cap. And also calculate which is the time of this Tcharge.
For instance Qg=5nC, Tsw=476,2ns-->Tcharge=47,6ns( considering 10% sw)
Igate=5nC/47,6ns=105mA
2.-Does the boostrap cap have another discharge/leakage current that should be taken into consideration apart of Igate of HS mosfet
3.- Which is the min voltage acceptable to be maintained on Cboot?
that means which is the mosfet Vgs voltage threshold?
4.-75ohms Rboot is the max value ?
how we could calculate which could be the limit?