This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM846C23: Alternate Part suggestion

Part Number: TPSM846C23
Other Parts Discussed in Thread: TPSM846E25, TPS546E25

Tool/software:

Hi,

We need a power module with below specifications.

1)Input voltage -5V

   Output voltage-0.68V

   Load current-100A

With PMbus feature and output voltage margining provisions. It can be either single module or stacked module with lower ripple and better transient response.

2) Input voltage-5V

    Output voltage-0.75V

    Load current-60A

With PMbus feature and output voltage margining provisions. It can be either single module or stacked module with lower ripple and better transient response.

Thanks

S Sathya shree