This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5180-Q1: Inquiry on operating characteristics at low power

Part Number: LM5180-Q1

Tool/software:

Hello. I have a question about the low voltage characteristics of the LM5180-Q1 product.

I was design 15V outputs 1CH circuit. (refer to Datasheet 9.2.2 Design 2)

The datasheet shows application curves from 12V to 65V, but there is no graph for low voltage.

I need characteristic curve about 5V and 9V.