This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS551892-Q1: [ZF] Load dump

Part Number: TPS551892-Q1
Other Parts Discussed in Thread: TPS552892-Q1

Tool/software:

Dear team,

The maximum input voltage of TPS551892-Q1 is 27V. What is the 12V output voltage performance under load dump (35V)? Thanks!

Regards,

Mingkang

  • Hi Mingkang,

    It depends on whether the device needs to operate or can be shutdown under load dump condition, if the max operating input voltage of the customer system is below 27V, then TPS551892-Q1 is suitable here.

    Otherwise, TPS552892-Q1 with operating input voltage until 36V is more suitable.

    For any price request, please reach out to our MKT team.

    BRs,

    Bryce