Part Number: TL783
Other Parts Discussed in Thread: TL081, LM324, LM324LV
Tool/software:
Hi,
I have a new design which has 60V constant output voltage and maximum 0.5A current value. But when I connect the load 60V value changes 59.8-59.9V. So I want to adjust the Vout and closed loop control. I used pwm to get analog output and single supply amplifier to set voltage like Figure 18. When I use single supply opamp (Zero drift), I can not adjust the output voltage. If dual supply power is used, it can be adjust. I can not use dual supply in my design. Is it possible to adjust regulator voltage with single supply opamp, or any other solution like switching regultor.