This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM36922: How to connect pins when using I2C control.

Part Number: LM36922

Tool/software:

Hi team.

Could you answer the following questions?

How should the PWM pin be connected when using I2C Only mode? (NC or pull down via resister?)

According to Table 1 in Datasheet, it seems like LED current is controlled by I2C command in case of PWM input is none,

However, the pin function description does not refer to connecting the PWM pin when using I2C control only.

Tsubasa.