Tool/software:
Hi Team,
Bq34z100-G1 is used for a 15cell LiFeP04 battery pack project. Current design's nominal voltage is 48V (15x3.2V) and capacity is 100Ah. So calculated design energy is 4.8kWH. As you can see in the belopw picture, design energy in mWh. Design energy scale is between 0-255. Design energy is between 0-5400. Even if maximum values are chosen , calculated design energy is 4800*255=1 224 000 mWh.
If design energy is calculated using one cell parameter, design energy is 3200mV*100Ah=320 000mWh. So design energy selects 3200 and design energ scale selects 100. Is this correct? I'm not clear about this register. Could you explain how can I calculate design energy? If it is a possible coul you give me a example for 15 serices cell 100Ah?
Thanks for support