This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3845: Required Inductor design for DC-DC Buck Converter

Part Number: UC3845

Tool/software:

Dear TI Expert,

We are designing dc -dc buck converter using UC3845.

Please help to design inductor for the following parameters.

 1. Input Voltage Range - 30 to 72 Vdc.

2. NO load Output Voltage - 13.80Vdc

3. Output current - 15A 

4. Frequency - 60 KHz

Remark: We have to use toroidal Core (KS130-125A) which have OD-34mm & Height -11.5mm.

This core is suitable for this design if it is not okay,

Please suggest core details, No. of wire turns, wire gauge and Inductance value

Thanks 

Rahul Sharma