Tool/software:
The device keeps restarting by means of coding. During this process, it charges for 5 minutes and then does not charge for another 5 minutes, repeating this cycle continuously. After running for more than 10 hours, the device failed to charge. Through actual testing, it was found that the charging current was only 10mA, and the internal VINDPM register value was 7.04V. This led to the fact that the 5V adapter basically did not output any charging current. This register is set to run by default on our side and will not be rewritten. Let's check if there is any direction for improvement here.