This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5812: I2C Slave Conflict Due to Broadcast Address on LP5812 – Is There a Way to Disable It?

Part Number: LP5812


Tool/software:

I'm experiencing an I2C slave conflict on the bus, potentially caused by the LP5812 using the broadcast address. Is there a way to disable or modify the broadcast settings on the LP5812 to resolve this issue? If not, can you suggest alternative peripherals with the same footprint that don't use a broadcast address?