Tool/software:
Dear *,
we wan to use LMR60440 but currently we can't find the part in WEBENCH to do the simulation.
Vin =24V
Vout =8V
Iout = 3A
L = 3.3uH XGL4020-332ME
Can you provide the efficiency graph from 0.5A to 3A for the upper parameters
Fsw should be adjusted in order to use upper inductor and have max efficiency.
Best Regards,
d.