Tool/software:
Hi ,
I AM DEVELOPING A DC DC CONVERTER OF INPUT 16 TO 36V AND OUPUT CONSTANT 24V/7A. WITH FSW 200KHZ USING LM5030 IN PUSH PULL CONFIGURATION
BUT WHEN THE CONTROLLER OUTPUTS IS NOT CONNECTED TO THE GATE OF THE MOSFETS I AM GETTING MAXIMUM AND CLEAN PULSES OF MAX DUTY. BUT WHEN I CONNECT THEM TO THE MOSFET GATES, OUTPUT 2 IS COMING MAX DUTY AND OUTPUT 1 IS COMING MINIMUM DUTY.
I WILL SHARE THE WAVEFORMS OF IT BELOW.

CS AND OUT2

OUT1 AND OUT 2
CAN YOU FIND WHAT MIGHT BE THE ISSUE THATS CAUSING. AND
THE APPLICATION CIRCUIT IS SAME AS FIGURE 8 OF THE DATASHEET WITH SOMKE TUNING FOR MY APPLICATION.
THE TRANSFORMER IS EE25 TDK
AND THE PRIMARY TURNS ARE 4 AND SECONDARY IS 6 AND BIAS WINDING IS 3.
ITS CENTER TAPPED PRIMARY WITH TWO WINDINGS OF 4 TURNS EACH AND CENTER TAPPED SECONDARY WITH TWO WINDS OF 6 TURNS EACH.
CAN YOU SUGGEST WHAT ARE MIGHT BE THE POSSIBLE REASONS THATS CAUSING THIS. SO THAT I WILL CHECK ALL THOSE.
LM5030 100-V Push-Pull Current Mode PWM Controller datasheet (Rev. D)
THANKS.