Other Parts Discussed in Thread: TPS25751
Tool/software:
Hello
Were can I download TPS65994AD reference manual for register & command details?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello
Were can I download TPS65994AD reference manual for register & command details?
Hi,
Can you outline the power and data capability you need? Do you need to pass PD compliance? I can provided device recommendation based on the information.
Regards
Hello
・45 W Power Supply
・USB2.0 support for data functions
・Device side to host side
・USB2.0 communication between host devices
We already have a board with TPS65994AD.
I need to run TPS65994AD, so I would like you to provide the necessary reference manual.
Hi,
I would recommend moving to TPS25751 if you need single port charging and USB2 data. We don't support 45W sourcing on TPS65994AD.
Regards
Hello
The desired configuration is as follows.
Port 1 will coordinate with the mobile battery's PD via CC communication, receive 15V/3A from the mobile battery, and send that power from Port 2.
Port 2 will coordinate with the counterpart device's PD via CC communication, and perform USB communication and power transmission.
I have been introduced to the TPS65994AD for the above conditions.
The board has already been created with it.
It would be troublesome to be designated a different device now.
This issue can be resolved if I receive the necessary information to operate the TPS65994AD.
Hi,
Do they need to pass USBIF compliance? If yes, they cannot use TPS65994AD.
Regards