This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79731-Q1: Bq797xx application doesnt run on my laptop

Part Number: BQ79731-Q1

Tool/software:

Hello,

I have the same issue with the BQ797xx-Q1 Installer version 2.0.3. After installation the application just doesn't run on my laptop HP EliteBook series with win 11. I have tried it with win 10 but the same thing.

It is just not execute. I have seen there is a tread regarding the Bq79718 which is solved but I am not able to see the solution for the fix.

Please advice!

  • Hi Bucur,

    Could you please specify the procedure when you are doing in installing the BQ797xx-Q1 GUI. 

    Please check if a computer restart would change the application behavior. As a workaround, please use BQ797XX, which is an online GUI version. Note that the online version would require additional installation of TI Cloud Agent.

    Best Regards,

    John