Tool/software:
Hi,
we are conducting tests by modifying the values of "Load mode" and "Load Select". We are testing with the following configuration:
- LoadMode=1
- Load Select=6
- Design energy scale=10
- User-rate-mA =6000
- User-rate-Pwr=12800
We have a load of 6A, with a voltage of 25.6V, which results in a total of 128W. For the (Load mode = 1 & Load Select = 6) configuration, we have modified the "Design energy scale". Could modifying this value affect other parameters of the "GoldenImage" and the system's operation?
Regards,