Tool/software:
Hi, 
Can you tell me if the issue has been resolved, as I have exactly the same problem ?
Is this component compatible with the use of a 12V battery ?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi, 
Can you tell me if the issue has been resolved, as I have exactly the same problem ?
Is this component compatible with the use of a 12V battery ?
Thanks
Hi,
This device can be used with 12V battery.
What is your schematic?
Thanks,
Colin
Hi,
Completely randomly, my component glitches when I connect my board to a 12V lead-acid battery (NP7-12 Yuasa).
Thanks

Hi Richard,
Are you using long wires to connect it to the battery. If yes, you should add a large EC capacitor at the input.
Because the long wire acts like an inductor and resonates at the input. This can cause VIN to be greater than 17V and damage the device.
Colin
Hi Colin, 
Thank you for your reply.
 I am using short wires (30cm).
 I will add a capacitor as you suggested, and I am also considering adding a resistor in series (20 Ohms) on the +12V to dampen the input signal.
 What do you think?
 Do you have any other ideas?
 Thanks in advance.
Hi Richard,
I don't think 30cm is considered a short trace. I think it's a testing issue and won't occur in real applications.
It's better to add a 1 ohm resistor to the 12V trace and add an EC capacitor for damping.
Colin
In my real application, the installation will be identical.
 I will try with the resistor and the capacitor. 
Can I also add a freewheeling diode?