Other Parts Discussed in Thread: TPS25751, TUSB320
Tool/software:
I am trying to design a system that connects an iPad to a ADC/DAC through a USB-C Port. The iPad should power the 5V_Bus in this configuration.
I have a second USB-C port to attach an optional external power source. When attached, the iPad should negotiate with the Power Supply to charge at up to 20V@3A. The Power Supply should also power the 5V_Bus.
My current design is below. I think it is mostly correct, however, I am getting the impression that the TUSB is the wrong part for this application. I also wonder if this is over engineered.