Tool/software:
Hello, I'm a student completing my first buck-boost converter design. My specs are as follows:
Vin = 10-19 V
Vout = 12V
I(max) = 5A
Before I ordered my PCB, I wanted to verify a few things I had questions on:
1. Is the resistor + capacitor at the COMP pin adequate? This is what the Webench circuit designer created for me, but other schematics I have found online have higher resistance values as well as a capacitor in parallel with the series RC.
2. Do I need a snubber circuit on each side of the inductor?
3. Is the output capacitance adequate for a switching frequency of about 400 kHz? I want ripple to be as minimal as possible.
4. Does the DITH/SYNC pin require a capacitor between it and GND?
Please let me know if anything else about the schematic looks off. Thank you!