Part Number: LP5860T
Other Parts Discussed in Thread: LP5860
Tool/software:
Hello guys,
One of my customers is going to evaluate LP5860T (Max current 100mA version) for their new products.
At this moment, they have the following questions.
Could you please give me your reply?
Q1.
Can LP5860T operate without any problem when the constant current at CSx pin is set to 100mA and PWM is 100% with 5V VLED?
Is any derating needed? Or is there any concerning point they should care?
Is it the device temperature?
Q2.
How much is Rsw(High-side PMOS ON resistance) when Isw is 1.8A(100mA*18ch)?
They didn't find the data in LP5860T datasheet. They concern that larger voltage drop would be occurred at SWx
because Isw is larger than LP5860 (Max current 50mA version).
The datasheet says that Vsat of CSx is 0.8V. If SWx voltage drop from VLED is 1V, the applied voltage to LED becomes 3.2V(5V-0.8V-1V).
They think that LED which has Vf less than 3,2V should be used for the case.
Your reply would be much appreciated.
Best regards,
Kazuya.