This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61022: Replacement for LT8349

Guru 10910 points
Part Number: TPS61022

Tool/software:

Hello,

My customer is looking for a boost solution for handheld device.

Please recommend the most suitable replacement for LT8349 based on the criteria below.

 - The input is 1 cell battery

 - It would be better if the maximum VOUT is close to 6V

 - IOUT should be 6A or more.

 - It would be better if the product supports the true shutdown function.

Thank you.

JH