This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22958: MAX CURRENT THROUGH THE BODY DIODE OF THE INTERNAL MAIN MOSFET

Part Number: TPS22958


Tool/software:

Hi, 

I expect to use TPS22958DGNR as the load switch to cut the connection between a 1-cell Li-Ion Battery and a BMS circuit for one of my projects.

When the battery is up for charging, the supply/main current should flow through this Power switch IC (Through the BODY DIODE OF THE INTERNAL MAIN MOSFET), and for that, I want to check whether the body diode that I mentioned before, is capable of handling that current (Around 3A at MAX).

Thanks.