Other Parts Discussed in Thread: TPS25751, TPS55288, PMP40801, TPS65987, BQ25758
Tool/software:
Hi,
in the meanwhile, the TPS65987D part has become status "is not recommended for new designs" and the TPS25751 is proposed as replacement for new designs.
However, currently available information and reference designs suggest that the TPS25751 supports external battery charger controller ICs only.
Since the TPS65987D was paired in some reference designs with the TPS55288 and initial idea was to use and adopt the PMP40801 reference design with TPS65987D I have several questions:
- Can the new part TPS25751 be paired with buck-boost converters such as TPS55288 or it supports solely battery charger controllers?
- Can we get the roadmap information for the TPS65987D part and other USB-PD controllers from TI?
- When it be the End-of-Lifecycle for the TPS65987D?
- Can the battery charger controller be used and operate as standard buck-boost converter, it means without connected cells?
We need the solution for the USB-C PD, 65W, 10~28V input voltage with following roles:
- power mode role: DFP (Source only)
- data mode role: UPF (Device only)
Do you have any suggestions how this can be implemented with TPS25751 device?
If the TPS25751 is not suitable for this application do you have any other part that fits here?
BR
Josko