Other Parts Discussed in Thread: TPS65987
Tool/software:
你好
CH347T IC 可以與 TPS65987DDHRSHR IC 通信嗎?
謝謝!!
德里克
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
No, the TPS65987 does not communicate SPI with anything other than a SPI Flash used for storing the config. There TPS65987 is not capable of communicating UART with the CH347 either.
Please understand that the TPS65987 does not act as a USB endpoint, and does not do anything regarding Data on the USB2 lines.
The USB2 (D+/D-) connections on the TPS65987 are only used for supporting BC1.2, a legacy USB-C charging scheme. If BC1.2 is not needed, you can disconnect these pins.
Thanks and Regards,
Chris