Part Number: LMZ10504
Tool/software:
Hello,
Regarding the component LMz10504TZX-ADJ/NOPB I need to know if the data code is printed on the component.
If yes i need to code how to read it.
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMZ10504
Tool/software:
Hello,
Regarding the component LMz10504TZX-ADJ/NOPB I need to know if the data code is printed on the component.
If yes i need to code how to read it.
Thank you
Hi Pietro,
Thanks for contacting us.
Date code information can be retrieved from the component marking. However, how to decode the component marking is TI proprietary information.
If you have concern about a particular component / batch, please provide the XXXXXX string according to the component marking that should look like below. We should then be able to provide you the corresponding date code.
+--------------------+
! !
! XXXXXXG3 !
! LMZ10504 !
! TZ-ADJ !
! !
! O !
+--------------------+
O - PIN 1
Thank you
Yann
Hi Yann,
Thank you.
The batch presents on the component is 45COLVG3 (see attached picture)
Which is the data code?
Do you have the rules to read the data code?
Best regards
Hi Pietro,
The corresponding date code should be May-2024 for this component.
As mentioned previously, the rules to read date code from component marking are TI proprietary and cannot be shared.
Thanks and best regards,
Yann