This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: bq28z610

Part Number: BQ28Z610
Other Parts Discussed in Thread: GPCCHEM

Tool/software:

Hi,

I am currently using the BQ256720EVM board with a 2-cell Li-ion battery configuration (3.7V, 4000mAh). While monitoring the system through Battery Management Studio (BMS), I observed the following issues:

  • Battery Percentage Display:
  • Although the voltage, current, and temperature values are displayed correctly, the battery percentage always shows 100%. Could you please provide detailed guidance on configuring the battery percentage accurately?
  • Chemistry Selection:
  • Considering I am using Li-ion 3.7V 4000mAh batteries in a 2S configuration, which battery chemistry profile should I select in BMS for optimal performance?
  • GG.CSV File Request:
  • If you have a working gg.csv file suitable for a 2S Li-ion configuration, I would greatly appreciate it if you could share it.
  • Voltage Calibration Issue:
  • During voltage calibration, I encountered an error indicating that "Cell 1 voltage is out of range." Could you please advise on the correct values and steps required for proper voltage calibration?

I would be grateful if you could provide point-by-point guidance to help resolve these issues effectively.
Thank you for your time and support.

Regards,
Syam