Other Parts Discussed in Thread: TPS923650
Tool/software:
Hello E2E,
I have the TPS922051/0 that allows a buck/boost configuration. When in this configuration, it will not boost when the Vout-Vin is more than 5V. Are there certain restraints with this configuration that does not allow a larger boost voltage?
Example - I have the eval kit TPS923650D2DRLRE VM with these parameters
Vin - 12VDC
VLED - 28.6VDC
ILED - 0.5A
With these parameters, I can only get 350mA output but when the Vin voltage is increased to 23VDC, the current is 508mA. The Vref @ 350mA is 130mV so it looks like the reference voltage is being affected by the large Vout-Vin difference.
Another question about the calculations on the datasheet. What is IL (Inductor Max) referring to? Is this MAX current that the inductor will see? Is it ILED with a 30% ripple? I cannot get my inductor calculations correct to try and troubleshoot the above issue.