This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS798-Q1: What is the max possible capacitance on the output?

Part Number: TPS798-Q1

Tool/software:

Hi,

I want to use 180uF capacitor on the output. Will I have a problem with stability?

I will also have a smaller low ESR cap as recommended by the datasheet too.

  • Hello,

    A larger output capacitor should be fine:

    "Larger values of output capacitance decrease the peak deviations and provide improved transient response for larger load current changes."

    Hope this helps!

    Best,

    Hannah