Other Parts Discussed in Thread: BQ25731, , TPS25751
Tool/software:
Hi Ti Team
If I use Type-C input voltage (PD Max 100W), will it use BATT (TP3) as the output?
Can I pin out a wire from the TP3 pin and charge a device, such as a tablet or laptop?
If it is Default's TPS25750EVM, what is the voltage range that BQ25731 can output?
Is it adjusted according to the picture below? or I need to rewrite the firmware using the GUI?