Tool/software:
The SS/TRK pin on the LM5146 contains clamping circuitry to limit the voltage to 115mV above the FB pin voltage. What is the maximum current that this clamp can handle? We are planning to connect SS/TRK to a DAC to create a variable voltage supply so we need to size an input resistor according to this limit.