Other Parts Discussed in Thread: BQ76907, BQ25756E, EV2400, BQSTUDIO, BQ41Z90
Tool/software:
Hello TI team,
Recently I used your BQ25756E chip to build a lithium battery charging circuit, I want to add a battery equalization module on the basis of this circuit to make the battery in the charging process to achieve the balance of the charging function. Currently I have noticed two chips:BQ40z80 and BQ76907, now I have the following questions.
1. Since I have less experience in digital programming, I would like to ask which one of these two chips can make it easier (e.g. without programming but using default settings) to equalize the battery during charging?
2. Can these two chips be directly connected to bqstudio via EV2400 for setup without the need of an MCU chip and peripheral chips?
3. Can you offer a better alternative? Currently I have 2-6 rechargeable batteries.
Thanks in advance!