Other Parts Discussed in Thread: LM5157
Tool/software:
Hello,
in snva994a application note page 4, the transformer's PRI inductance is calculated as 13 uH, and it says for normal operation they are going to use CCM, but when selecting a value for CCM operation, they have to choose 8 uH. Why is that? Won't that push the converter in DCM??
Also on the same page, it says this - ILPEAK is used to properly size the current sense resistor.
Where is the circuit current sense resistor used? Am I missing something? I thought it was internal?
Thanks and Regards,
Naveen