This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM82901: Max output capacitance question

Part Number: TPSM82901
Other Parts Discussed in Thread: TPSM82902

Tool/software:

Hi,

In the datasheet max output capacitance is rated at 100uF directly at the output of the device. What does that mean actually for the capacitance located for example 20mm further away?

I read here on the forum that 400uF is ok for TPSM82902 which has the same specs on datasheet. Just wondering if I dare to place around 340uF of capasitors to 1.2V output for FPGA. With that DC bias it would actually be around 240uF probably.

Best regards,

Petteri