Part Number: TPS55340
Tool/software:
The Css value is suggested to be "The Css can be from 10nF to 0.22uF, depend on your needs.". There is also an appnote that Css is based on different topologies.
If I am using the TPS55340 in boost topology, are the limits on the Css values the same as told?
If larger capacitance value can be used in boost topology, how large is the upper limit?
Regards,
Tai