Hello, I am trying to get a UC2856 Ic to work properly at no load and light load conditions. The problem I am having is that once the on time wants to drop below around 1us it starts to skip gate drive pulses randomly. I have tried a number of different configurations and I can't seem to get a linear response on the lower end of my slope compensation even without running power at all. The ramp looks clean and smooth (at least without load).
Any suggestions?
Configurations tried:
Changing EA- voltage from 1.7V to 2.5V to 3.92 V and down to 1.2V.
Changing slope seen on CS- to CS+ 1st (0 - to 100mV) 2nd (0-200mV) and (100mv to 500mv slope)