Other Parts Discussed in Thread: TPS2559
Tool/software:

I have connected the HD3SS3220 port controller between a USB hub and a USB type C connector. I know my hub can enumerate SS devices on its other ports but on the port with the Port controller and Type C it only enumerates a device as HS mode and only in one direction (if I flip the connector it only works one way). I thought maybe I needed to force it to DFP mode by connected the PORT pin to 5V but that didn't help either.
Can you tell me if you see a problem with my schematic? thank you!
Jonathan