Other Parts Discussed in Thread: TPS7H4011-SEP, TPS7H2140EVM
Tool/software:
Hi,
I am currently working on Latching Current Limiters (LCL) based on the TPS7H2140-SEP for a Power Conditioning & Distribution Unit (PCDU) for a satellite. The input voltage requirement imposed is 22V-34V, whereas I see that the component is rated for up to 32V. My main question concerns the tripping and current limiting response times. Can these timings be controlled at the component level? I don't see where this is mentioned in the datasheet. If it is possible, how can it be implemented? This function is critical for our LCLs.
Another question: If I want the component to operate in auto-retry mode (automatic restart after a trip) or in latch-off mode (requiring a command to restart after a trip), how do I configure it? These are standard functions for LCLs.
Thanks in advance for your support.
Best regards,
Mouhameth