This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need Alternative Boost Converter with 7VDC Output

Part Number: TPS61253
Other Parts Discussed in Thread: TPS61372

Tool/software:

My company uses the TPS61253 boost inverter in a production device.   This posting is a request for an alternative TI part that behaves similarly to TPS61253 but has these additional features:

  • has ability to output +7VDC, even if external voltage setting resistors are required
  • comes in a real world package, not the unmanageable DSBGA package the part uses now

These are my overall needs:

  • Voltage adjustable boost inverter
  • one lithium ion cell input voltage (~3.5V)
  • 7V@300mA output
  • Ok if the device has no output switch
  • Any temperature range is OK

Preferred package type is 3mmx3mm WQFN or at least 9mm footprint

Jim Olson
Curative Sound LLC
Carmel, IN US