This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5148: LM5148RGYR output loss Vs high load

Part Number: LM5148
Other Parts Discussed in Thread: CSD19532KTT

Tool/software:

hello

i used the LM5148RGYR to regulate 38-45V input, to 24v/5A output. 

when the load is high (3A and higher) the output voltage drops to 23.4v down even to 23v 

what can be the reason?

Can i fix it ? or only increase the regulated output, compensating the voltage lost  

(The FET's i used are BSC105N10LSF_G + CSD19532KTT &  coil Vishay__IHLP_6767GZER220M11  )

Thanks in advance

Doron