This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6521905: Using the Internal LDO for 2mA external usage

Part Number: TPS6521905

Tool/software:

Hi, 

I know that it clearly says we shouldn't power external circuitry in the datasheet for VDD1P8 pin of TPS6521905. However, If I can draw 2mA, I can save an extra LDO on the circuit. Therefore, I can save some cost and space. 

So, it is possible to draw max 2mA on pin VDD1P8?

Regards,
Caner