This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6521905: Discrete Power Solution Suggestion for LPDDR4 or LPDDR4X

Part Number: TPS6521905
Other Parts Discussed in Thread: TPS65296

Tool/software:

Hi,

I use a PMIC but the number of outputs are not enough. I need a discrete power solution for a single LPDDR4 or LPDDR4x. There are two rails, 1V1 (VDD2)) with 1A max and 0V6 (VDDQ) with 0.6A max. 

Can you please suggest a solution? 

Vin is 5V. I will need enable pin to control the power sequence. Small size is desired, even WLCSP or small QFN. It would be nice if I can use the same part number for both rails. 

Regards,

Caner