This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65262-2: Max PGOOD current

Part Number: TPS65262-2


Tool/software:

Max PGOOD current isn't specified in the datasheet. One of the test conditions indicates 1mA is acceptable.

And section 7.3.11 recommends a pull up resistor between "10 and 100 kohms to a voltage source that is 5.5 V or less", indicating that 550 uA is acceptable.

However, I would like to sink ~5mA into PGOOD-- enough to drive a BJT with enough margin to support a heavier load.

Can you tell me what is the max current PGOOD can sink for high reliability and long life over temperature extremes?

Thanks.