Tool/software:
Howdy,
I am considering designing with this energy harvester and am a little confused about possible input sources. The recommended designs show high input impedance sources such at TEG's or solar cells or vibration elements.
I am wondering if there is some design limitation whereby very low input impedance sources can not be used. In the intended application, the output storage element is a 4.2v LiPo. Specifically I am energy harvesting from disposable batteries which, when fully charged, have an ESR of around 100mΩ and drop to approximately 2Ω when nearly depleted - all very low as compared to the recommended input devices ESR's all in the MΩ's I think.
The question is: can very low input impedance sources be used as power inputs with this part WITHOUT a series resistor? I haven't found anything that would suggest this would not work, but the EVM notes say to use at least a 100Ω in series with the input voltage source when using a bench power supply. A little confused about this...
Any advice is appreciated.
Thanks,
Kevin
bard-designs.com