Tool/software:

I am needing to be able to turn on AND off the last scan line pulse from the round robin sequence. I think the only way to do this is to modify the 'Max_Line_Num" field in the Dev_initial register. I do not know if this is permitted in operation (i.e. chip enabled) nor do I know if this will affect the brightness of the remaining LEDs as the round robin is changing between 7 and 8 states.