Tool/software:
I would appreciate your help regarding the times in the attached image.

Can the min/ max Duty Cycle be calculated based on these times using the following equations?

For example, if I want D=98% and T_sw=5usec, so ton=98%*5usec=4.9usec and t_off= 100nsec. Is this scenario possible?