Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM
Tool/software:
Hi,
I'm trying to complete the learning cycle for our 4S5P LFP pack, based on the procedure described in SLUA903.
The cells are JGNE 18FC-5 type, 3.2V, 1600mAh. They went trough TI testing recently and now they have an official ChemID of 4207, and this chemistry is set in the gauge.
Settings:
Design Capacity mAh: 8000
Design Capacity cWh: 10240
Design Voltage: 12800 [mV]
Charge Term Voltage: 75mV
Charge Term Taper Current: 50mA
*The current and voltage calibration is done, the gauge reports accurate readings.
With a fully charged battery pack, I started the learning cycle.
- first part of discharge with 1A is done, the DOD0 values got updated. According to the gauge, the capacity is around 8400mAh.
- As a second step, I charged the pack with 14.6V @ 4A, some time after the end of the charge the VOK register changed to 0 and the pack went into REST state. However, after this the QMAX register did not change to 1.
I would like to ask for help on what setting I have messed up, which is why the QMAX update cannot be completed and the update status is stuck at 04.
*I do have the mysterious IT Gauging 2 Configuration enabled in BQStudio, where the QMAX_EOC register was in "1" by default. I'm not sure if this is good or not, but some topics in this forum suggested that it may be needed for LFP cells.qmax_failed.gg.csvqmax_falied.zip5773.JGNE Goldencell JGCFR18650-1600mAh-3.2V-EN.pdf