Other Parts Discussed in Thread: GPCRB
Tool/software:
We are working on a project that uses the TI BQ27Z558YPHR DSBGA12 HF IC. During the low - temperature RBTweek test, the GPC report showed a Qmax is only 99mAh. This result was consistent in two separate tests. However, the battery has a capacity of 480mAh, and the gg file shows a Qmax of 490mAh after learning. Why is there such a discrepancy? Are there any potential risks involved?GPC_RB-report.zipGPC_RBtweek-report.zipGauging Parameter Calculator report for input file 'GPC_RB.zip'.msgGauging Parameter Calculator report for input file 'GPC_RBtweek.zip'.msg