Other Parts Discussed in Thread: TPS3899
Tool/software:
Hi
I am lookin for a low sensne current solution. when VDD =0.
it's for RTC battery sense
Does TPS3808 can I sense can keep <25nA when VDD =0

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dimitry,
For RTC battery sense application, I would recommend the TPS3899 instead of the TPS3808.
The TPS3899 has an Iq of 125nA in comparison to 2.4uA of the TPS3808. Also the TPS3899 utilizes a capacitor ladder for its fixed variant instead of a resistor ladder on the SENSE pin which would minimize the Isense even with VDD=0.
https://www.ti.com/product/TPS3899

Jesse
Hi Jesse
My design is vcc connect to main power.
and I only concenr about I sense current..
TPS3899 is not in my original design.
TPS3808 is my prefer part.
please help me to check I sense when VCC=0.
Hi Dimitry,
Are you using the adjustable variant, TPS3808G01, or the fixed variant, TPS3808GXX, of the device?
Jesse
Hi Dimitry,
With the TPS3808G01, Isense at VDD=0 is 0A and with VDD=VDD(min) Isense=~25nA. With this setup, the main concern is the external resistor ladder when VDD of TPS3808 is at zero.
Jesse