Tool/software:
Hi,
We are currently implementing a BQ24070 Linear Charger in an IoT based application. we have tested both 1.5K , 1k and 750 Ohms for the ISET1 value. According to the calculations , charge current should've been 708mA,1062mA and 1416 mA respectively. But we are only averaging about 350 mA in all cases. We have tested with both Li-po and Li-ion chemistries. Any help would be appreciated. Rest of the configuration values are default as per reference values given in detailed design procedure (9.2.2) in the datasheet.
Thanks