Tool/software:
Hello,
I am using LP2985 to regulate 5V to 5V and seeing a nominal current draw of 30mA from the regulator. Is this typical? If I replace Cbias with a 10kohm resistor the current drops to 7mA.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
I am using LP2985 to regulate 5V to 5V and seeing a nominal current draw of 30mA from the regulator. Is this typical? If I replace Cbias with a 10kohm resistor the current drops to 7mA.
Thanks,
Hey,
It seems to me that the problem is most likely that you're operating the LDO without enough headroom (5V to 5V). This is likely causing the pass element to saturate leading to higher quiescent current. An LDO is typically not recommended for applications where VIN ≈ VOUT.
Recommendations
1. Provide adequate headroom:
If you need a regulated 5V rail. VIN should be tens to a couple hundred mV above VOUT. See datasheet for exact dropout values for your situation.
For example, 5.3 to 5V
2.Use a load switch if regulation is not required
Hope this helps,
Vahnroy Hosear