This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BUCK-CONVCALC: Buck converter suggestion

Part Number: BUCK-CONVCALC
Other Parts Discussed in Thread: LM5169, LM5168

Tool/software:

Hello Team,

I am looking for buck converter to convert 16.8V to 154V input voltage to 12V output and output current requirement is 0.5A. Is it possible using available high side buck converter topology if yes which device is recommended for this ?

Thank you.

BR,

Vaibhav